MTRDEVKSBNK144 PreDRV Fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MTRDEVKSBNK144 PreDRV Fault

2,433件の閲覧回数
sohyunjang
Contributor III

Hi, I use MTRDEVKSBNK144.

I test the board, but PreDRV Fault was occurred.

tppDrvConfig.deviceConfig.statusRegister[0U] = 8

tppDrvConfig.deviceConfig.statusRegister[1U] = 73

tppDrvConfig.deviceConfig.statusRegister[2U] = 255

tppDrvConfig.deviceConfig.statusRegister[3U] = 0

I just connected the power(12V, 1.5A adapter), not run motor.

WhatWhat's problem??

Thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

1,986件の閲覧回数
Eugene3957
Contributor I

I figured it out it was due to wrong pin settings.
try to use J107 1-2 (use 12 v)

0 件の賞賛
返信