MC33772C IS_OL_ FLT ( Isenese Open Load) fault, How to get this fault S32K344 TPL PHY MC33665

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33772C IS_OL_ FLT ( Isenese Open Load) fault, How to get this fault S32K344 TPL PHY MC33665

819 次查看
jerryrig
Contributor III

Dear sir/madam,

I have interfaced MC33772CTC1 with S32K344 using TPL gateway MC33665. Software sdks i am using HVBMS bundle S32k344 specific BMS SDK which is BMS SDK 4.4 - R21-11 Version 1.0.2. 

 

With above setup i am able to get all gpio ADC voltages as well as some gpio i am using as gpio output also i am using ISense channel with shunt to measure current. All things working properly, Only thing which i want to enable right now is Isense Open load fault which is present in ( Fault status register 1 – FAULT1_STATUS ) bit no 5. I am able to get the data of this register using Bcc_772c_FEH_GetFaultStatus() api from CDD drivers of BCC_772c. Also i have enabled the FEG config regiter's IS_OL_FLT bit in processor expert.

Still i am not able to get the fault, i Am able to read the message content of response of Bcc_772c_FEH_GetFaultStatus() api in transaction descriptor but data doesnt changes even i after opening the SRP SRN connections it remains same.

can you please let me know what else i have to do to get the data. If any procedure sequence i am missing please let me know

@narsimh_kamath 

MC33772C, S32K344-WB , MC33665A 

Thanks.

0 项奖励
回复
2 回复数

787 次查看
narsimh_kamath
NXP Employee
NXP Employee

hi @Cristian_Durla - would you be able to advise on this query pls? 

0 项奖励
回复

756 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Aditya (@adijoshi),

As Cristian is OOO this week, could you help with this community question, please?

Thanks & BRs, Tomas

0 项奖励
回复