MAC address of S32K controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAC address of S32K controller

347 Views
rak14
Contributor III

Hi,

I'm using multiple S32K148 controllers with Ethernet feature.

In example code lwip_S32K148 the MAC address is .hwaddr = { 0x10, 0x11, 0x12, 0x77, 0x77, 0x77 }.
Can we change the MAC address to different for different controllers?

Is there any constrain to use the particular Mac address?

0 Kudos
Reply
1 Reply

327 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes you can, or better you should. Each device on your LAN should have unique MAC address.

Check web for MAC address composition.

BR, Petr

0 Kudos
Reply