S32K144 Reconfigure disabled Watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Reconfigure disabled Watchdog

650 Views
DynamicsNoDriver
Contributor I

I want to reconfigure the watchdog of the S32K144 after it has been disabled in the startup script. In the startup script there is following section that disables the watchdog:

 

/**************************************************************************/
                      /* WDOG DISABLE*/
/**************************************************************************/
  
#if (DISABLE_WDOG)
  /* Write of the WDOG unlock key to CNT register, must be done in order to allow any modifications*/
  WDOG->CNT = (uint32_t ) FEATURE_WDOG_UNLOCK_VALUE;
  /* The dummy read is used in order to make sure that the WDOG registers will be configured only 
   * after the write of the unlock value was completed. */
  (void)WDOG->CNT;

  /* Initial write of WDOG configuration register:
   * enables support for 32-bit refresh/unlock command write words,
   * clock select from LPO, update enable, watchdog disabled */
  WDOG->CS  = (uint32_t ) ( (1UL << WDOG_CS_CMD32EN_SHIFT)                       |
                            (FEATURE_WDOG_CLK_FROM_LPO << WDOG_CS_CLK_SHIFT)     |
                            (0U << WDOG_CS_EN_SHIFT)                             |
                            (1U << WDOG_CS_UPDATE_SHIFT)                         );
                            
  /* Configure timeout */
  WDOG->TOVAL = (uint32_t )0xFFFF;
#endif /* (DISABLE_WDOG) */

 

  

If later on i try to reconfigure the watchdog which should be possible because the Allow Updates field of the Watchdog Control and Status Register is set, the watchdog configuration does not change. I use the following code:

 

    DISABLE_INTERRUPTS()
    WDOG->CNT = 0xD928C520U; // Unlock watchdog
    while (!(WDOG->CS & WDOG_CS_ULK_MASK) != 0u)
        ;                           // Wait for wdog to be unlocked
    WDOG->WIN = 0x0000;
    WDOG->TOVAL = 50;
    WDOG->CS |= (WDOG_CS_CLK_MASK & (1 << WDOG_CS_CLK_SHIFT));
    WDOG->CS |= WDOG_CS_INT_MASK;
    WDOG->CS |= WDOG_CS_EN_MASK;
    while (!((WDOG->CS & WDOG_CS_RCS_MASK) != 0u))
        ; // Wait for config to be changed
    ENABLE_INTERRUPTS()

 

If I enable the watchdog on startup with this code:

 

  /* Write of the WDOG unlock key to CNT register, must be done in order to allow any modifications*/
  WDOG->CNT = (uint32_t ) FEATURE_WDOG_UNLOCK_VALUE;
  /* The dummy read is used in order to make sure that the WDOG registers will be configured only 
   * after the write of the unlock value was completed. */
  (void)WDOG->CNT;

  /* Initial write of WDOG configuration register:
   * enables support for 32-bit refresh/unlock command write words,
   * clock select from LPO, update enable, watchdog disabled */
  WDOG->CS  = (uint32_t ) ( (1UL << WDOG_CS_CMD32EN_SHIFT)                       |
                            (FEATURE_WDOG_CLK_FROM_LPO << WDOG_CS_CLK_SHIFT)     |
                            (1U << WDOG_CS_EN_SHIFT)                             |
                            (1U << WDOG_CS_UPDATE_SHIFT)                         );
                            
  /* Configure timeout */
  WDOG->TOVAL = (uint32_t )0xFFFF;

 

I can reconfigure it later with the same reconfiguration code above. Is reconfiguration only possible when the watchdog is enabled?

0 Kudos
Reply
3 Replies

629 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DynamicsNoDriver,

Can you write WDOG->CS in just one write?

 

BR, Daniel

0 Kudos
Reply

621 Views
DynamicsNoDriver
Contributor I
Hello @danielmartynek,
this works for me. Can you please explain why I need to write WDOG->CS in one write when the watchdog was disabled previously but it's possible to write to WDOG->CS multiple times when the watchdog was enabled before?
0 Kudos
Reply

617 Views
danielmartynek
NXP TechSupport
NXP TechSupport

The WDOG stays unlock for just 128 BUS_CLK cycles.

You need to make sure the CS register gets written within the window.

 

Regards,

Daniel

 

0 Kudos
Reply