Library for secure boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Library for secure boot

2,016 Views
Roh
Contributor I

I am going to use Bootloader's Secure Boot for the CSEc Security Module on the S32K146.


The usage of CSEc was confirmed through AN5401 example code.


However, there is no Source Code for Secure Boot Process.


1. Can I get a Secure Boot Library?

 

2. if Lib not exist, should I develop it?

 

Regards,

 

Roh

 

Secure boot 

0 Kudos
Reply
1 Reply

2,010 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Roh

        I don't know if you have the DEMO project code, here I will post a link, if you don't have one, you can refer to it.

AN5401SW-

https://community.nxp.com/t5/S32K/Who-can-share-S32K-secure-boot-sample-AN5401SW-zip/td-p/797807 

How to use-

https://community.nxp.com/t5/S32-Design-Studio/How-to-compile-AN5401SW-zip-in-S32-Design-studio-for-... 

Hope these reference routines can help you.

BR!

Jim.

0 Kudos
Reply