LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0

1,400 次查看
anoop_radhakris
Contributor II

Hi Jorge,

Thanks for the reply.I used LPUART2 module because initially

LPUART was not working properly with LPUART 1 using eval board(this is with

respect to normal echo example Iam telling without using processor

expert.).So i used LPUART2 instance with processor expert also. Are you

able to receive back whatever you are sending from serial terminal when you

tested?Also is there any issue if I use LPUART2 instance?

0 项奖励
回复
1 回复

1,295 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Anoop,

I checked the examples for LPUART for the S32K144 available in S32DS (with and without PE) and everything works well. 

Also, I'm able to use LPUART2 instance without any issue.  

I'm not sure what is not working on your side.

Best Regards,

Diana

0 项奖励
回复