LPSPI Manual Chip Select

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI Manual Chip Select

3,593件の閲覧回数
Aravind_Vinas
Contributor II

Hi, I am trying to configure my SPI2 port for operation using processor expert. But I see that there are already designated CS pins for operation. Could I configure the TCR register with PCS[0:3] and initiate transfer and manually control another GPIO pin as CS by pulling low? If so, what is the effect on the pin specified in the PCS field of the TCR register?

タグ(3)
0 件の賞賛
返信
6 返答(返信)

3,573件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is a possible but somewhat overcombined way. SPI transfer is initiated when CS is low but according CLK clock.

If you drive CS line manually by general purpose output, content of TCR[PCS] is irrelevant.

0 件の賞賛
返信

3,552件の閲覧回数
Aravind_Vinas
Contributor II

But the TCR[PCS] points to some CS line always. Which means the line being pointed will get low whenever a transfer is initiated. Or is there a configuration on the SPI registers where it can ignore the TCR[PCS] setting?

 
 
0 件の賞賛
返信

3,534件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, but it is internal signal. If there is no routing done by PORT module (this internal signal to pin), it does not have any relevance.

0 件の賞賛
返信

3,529件の閲覧回数
Aravind_Vinas
Contributor II

If I understand this correctly, if the pin is not routed as ALT function to serve as PCS using the PORT engine, then this TCR[PCS] shall not have any effect on the pin.

0 件の賞賛
返信

3,525件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you are right.

0 件の賞賛
返信

3,522件の閲覧回数
Aravind_Vinas
Contributor II

Kudos, thanks for the quick support!

0 件の賞賛
返信