Hi
https://community.nxp.com/t5/S32K/Implementing-LPIT-DMA-SPI-for-UJA1169TK-F-in-S32K144/m-p/1430149#M...
I was trying to implement the above implementation with the help of SDK(V3.0.0) for S32K144
I could manage to configure 2 DMA channels and link it with Tx & Rx of LPSPI
Once I start both the DMA channels , It is hitting Default ISR and throwing error as shown below

But the Tx & Rx is working perfectly , I can see the expected received value in array

I'm not sure , what's causing an interrupt , help me out
I have attached the project for the reference , Let me know if there is an issue
Best Regards
KARTHIK SV