LPSPI CLOCK LOOP_BACKED Mode application?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI CLOCK LOOP_BACKED Mode application?

1,806件の閲覧回数
JeorgeB
Contributor III

Hi,

 

RM of s32k14x for LPSPI module says (Page 1632):

"Enabling the loopback version of the LPSPI_SCK can improve the setup time of the input data from the slave"

what means this?

2. in datasheet, in LPSPI timing, Master LOOP_BACKED MODE :

Capture.JPG

why using loop backed mode will increase SPI operation frequency?

 

Thanks.

0 件の賞賛
返信
1 返信

1,799件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jeorge,

As shown below, the master can sample the MISO data using either the SCK ouput signal or the delayed SCK output signal.

danielmartynek_0-1605082223748.png

If the sample loopback is used, it improves the min. setup time.

danielmartynek_1-1605082308643.png

danielmartynek_3-1605082323657.png

 

danielmartynek_4-1605082333524.png

 

Regards,

Daniel