LPSPI CLOCK LOOP_BACKED Mode application?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI CLOCK LOOP_BACKED Mode application?

1,801 Views
JeorgeB
Contributor III

Hi,

 

RM of s32k14x for LPSPI module says (Page 1632):

"Enabling the loopback version of the LPSPI_SCK can improve the setup time of the input data from the slave"

what means this?

2. in datasheet, in LPSPI timing, Master LOOP_BACKED MODE :

Capture.JPG

why using loop backed mode will increase SPI operation frequency?

 

Thanks.

0 Kudos
Reply
1 Reply

1,794 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jeorge,

As shown below, the master can sample the MISO data using either the SCK ouput signal or the delayed SCK output signal.

danielmartynek_0-1605082223748.png

If the sample loopback is used, it improves the min. setup time.

danielmartynek_1-1605082308643.png

danielmartynek_3-1605082323657.png

 

danielmartynek_4-1605082333524.png

 

Regards,

Daniel