LPI2C behavior on the overrun condition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPI2C behavior on the overrun condition

2,284件の閲覧回数
james-lee
NXP Employee
NXP Employee

Hello team,

 

Would you please clarify the LPI2C behavior below in the slave mode?

 

1. Is the 4 depth of Rx FIFO available in the slave mode?

2. If not, in the overrun condition, does the following data overwrite the pending data? or is the following data discarded?

3. If the following data overwrites the pending data, when would it be done? After receiving the last bit of data?

4. If the STOP condition is detected during the data was pending, how does the LPI2C module behave?

 

Best regards,

James

0 件の賞賛
返信
2 返答(返信)

2,273件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello James,

 

1.

No, only the master features the FIFO.

danielmartynek_0-1620121651066.png

2 & 3.

This is not specified, but the LPI2C Slave supports clock stretching.

Refer to AN5301 Using LPI2C on KL28, Section 6.2. Configure stall

https://www.nxp.com/docs/en/application-note/AN5301.pdf

Or the S32K1xx RM, rev.13, Section 52.3.3.3 Clock Stretching

In both configurations, the LPI2C Slave stalls the bus (SCL held low) until the data are read and the transfer acknowledged.

 

4.

If the LPI2C slave receives a STOP condition, the SDF flag is set.

But again, the Master can't send a STOP condition while the bus is being stalled.

danielmartynek_1-1620122243530.png

UM10204 I2C-bus specification and user manual

https://www.nxp.com/docs/en/user-guide/UM10204.pdf

 

Regards,

Daniel

 

 

 

 

0 件の賞賛
返信

1,968件の閲覧回数
bobpaddock
Senior Contributor III
Is there any code, like a .zip file that goes with AN5301?
All I'm finding is the PDF.
0 件の賞賛
返信