LPI2C: Inverted SCL on S32k144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPI2C: Inverted SCL on S32k144

3,869件の閲覧回数
ArushThomas
Contributor III

Hi all,

I was trying to configure an S32k144 as an I2C Master, and seem to have encountered a bug. The SCL waveform is inverted (HIGH when it should be LOW, and vice-versa). I have observed this behaviour on my Oscilloscope;

  • pink: SCL
  • yellow: SDA

SCL_Invert.pngSCL_Invert.png

This behaviour is observed in Debug mode, when I disable all breakpoints and let the code run at regular speed.

 

When I step through the code line-by-line with the Debug features, I observe different behaviour

SCL_Correct.pngSCL_Correct.png

This is the waveform I had expected at all times.

  • The S32k144 is configured as a Master I2C device, and no other devices are present on the bus.
  • I am using the LPI2C0 peripheral, on pins PTA3 and PTA2.
    • Pins PTB7 and PTB6 are connected to an External crystal oscillator, so I haven't tested those.
  • External 4.7k pull-up resistors are connected to the SCL and SDA signals.
  • I have verified open-drain configuration of the pins, and all Clock settings.
  • Both the Blocking and Non-Blocking methods provide the same waveforms. [I2C_MasterSendDataBlocking() and I2C_MasterSendData()]

Here's the code;

Main.pngMain.png

EDIT: Added project "I2C_Reconfig.zip", which produces this issue

タグ(3)
0 件の賞賛
返信
6 返答(返信)

3,792件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ArushThomas,

The SCL signal is not inverted but shifted.

 

danielmartynek_2-1703165408513.pngdanielmartynek_2-1703165408513.png

 

danielmartynek_3-1703165420576.pngdanielmartynek_3-1703165420576.png

I could not open your project, because you use an older SDK, unfortunately.

Nevertheless, I could reproduce it with a simple bare-metal code.

We can see the shift when the LPI2C module is operational in active debug mode.

MCR_DBGEN = 0

danielmartynek_4-1703165612779.pngdanielmartynek_4-1703165612779.png

MCR_DBGEN = 1

danielmartynek_5-1703165638715.pngdanielmartynek_5-1703165638715.png

If you don't need the module active while the CPU is halted in debug mode, clear DBGEN.

 

Thank you,

BR, Daniel

0 件の賞賛
返信

3,695件の閲覧回数
ArushThomas
Contributor III

Hi @danielmartynek, thanks for your reply!

I've tried to implement your solution, here's my code;

 

 

I2C_MasterInit(&i2c1_instance, &i2c1_MasterConfig0);
LPI2C0->MCR |= LPI2C_MCR_DBGEN_MASK; //MCR value is set to 9
//LPI2C0->MCR &= ~LPI2C_MCR_DBGEN_MASK; //MCR value is set to 1
for(;;){
  I2C_MasterSendData(&i2c1_instance, masterTxBuffer, TRANSFER_SIZE, true);
  OSIF_TimeDelay(50);
}

 

 

 Probing the waveforms on my scope again, I'm not seeing any difference; the SCL waveform is still Shifted, whether MCR is 9 or 1.

As a sanity check, I set MCR_MEN to 0, to verify I was writing to the correct register. This completely stopped all waveforms, as I had expected. (Master logic is disabled)

 

Incidentally, I am not facing this issue when I set the Baud Rate to 400kHz; This issue only seems to present itself at 100kHz

Correct waveform observed @400kHzCorrect waveform observed @400kHz

0 件の賞賛
返信

3,680件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ArushThomas,

If the non-blocking API is used (I2C_MasterSendData()), we need to use the I2C_MasterGetTransferStatus() before we can call I2C_MasterSendData() again.

Can you use it?

 

Thanks,

BR, Daniel

 

0 件の賞賛
返信

3,835件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ArushThomas,

Could you attach the project here so that I can reproduce it?

Is the LPI2C module reporting any error during the test?

 

Thank you,

BR, Daniel

0 件の賞賛
返信

3,813件の閲覧回数
ArushThomas
Contributor III

Sure! I've edited my original post to attach the project .zip file

Is the LPI2C module reporting any error during the test?

I've used the status_t error variable to identify if any function returns an error status. All Init() functions return STATUS_SUCCESS. The I2C_MasterSendDataBlocking() function returns STATUS_I2C_RECEIVED_NACK. I expected this, since there is no Slave on the I2C bus.

The I2C_MasterSendData() function returns STATUS_SUCCESS. I did not expect this, I was expecting NACK again.

Is there some other technique I need to follow, to identify if the LPI2C module reports an error?

0 件の賞賛
返信

3,792件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Regarding the non-blocking method: The I2C_MasterSendData(),

The function completes before the transfer is finished, it does not block the core during the transfer.

We need to use this API: I2C_MasterGetTransferStatus() to get the expected STATUS_I2C_RECEIVED_NACK

 

Regards,

Daniel

 

 

0 件の賞賛
返信