I had downloaded the unified_bootloader_demo_v2.1 which contains demo applications of bootloader.
I want to use LIN S32K142 bootloader, but the demo project does not contain the project for LIN S32K142, so I converted the LIN S32K144 project to LIN S32K142. On flashing the bootloader project on the NXP S32K142 100 pin board, the LED pins toggle but we get the following error on ECU bus tool.
What should be done to resolve this?
@nxf10035
Greetings!!!
I am using S32K324 controller. I have developed non-UDS application.
I want to use bootloader software to flash non-UDS applicaiton.
[Query]
Is it possible to use unified bootloader [S32K324_CAN_Bootloader_RTD2d0 & ECU bus GUI] to flash non-UDS application? If yes, what software updates I will have to make in [S32K324_CAN_Bootloader_RTD2d0 & ECU bus GUI]?
Hi Tomlin,
Is it necessary to have UDS implemented in the application code to be flashed . As per my understanding once bootloader code is flashed we can flash application code via ECU bus using bin file even though UDS is not implemented in that .Please confirm my understanding .
Hi, @Asharm11
From your picture, I see that you only select download file process. Please note, the step as following:
1. Import process(JSON)
2. Connect hardware and config LIN node information
3. Select address of ECU BUS
For how to use the ECU-BUS, you can reference the user guide of ECU_BUS.
Suggestion you can open PLIN view and check the log of LIN BUS. It's better to upload the log when you met problems.
BR
Tomlin
Hello @nxf10035
I followed what you said and i have been referring the ECU bus User guide there is nothing for how to use UDS on LIN and the error remains intact
so can we have a meeting regarding this issue
I am sharing the PLIN view Image as well as current error's image
Hello @nxf10035
I changed the TX and RX ids to 3C and 3D respectively but I am getting the same result
I am attaching the snapshot for ECU bus tool setting and LIN tp settings
thank you
Abhishek
hello @nxf10035 ,
I tried with the IDs provided by you but I am getting the same error
and I am using the ECUBUS tool(0.2.13) ,could that be the issue?
I am attaching the snapshots of LIN TP settings
your thoughts would be appreciated
Thank you
Abhishek
Hello @nxf10035 ,
I used ECUBUS tool (v0.2.23) and still getting the same error "[4935ms][sch1]{"msg":"No response","index":1}"
could you please help me with it and Could you tell me how to generate the log file as well
Thank you
Abhishek
Hi, @Asharm11
The log captured by PLIN-View Pro. The test step:
1. Open ECU-BUS and connect PCAN(LIN)
2. Open PLIN-View Pro and capture the LIN log
3. Click Start of ECU-BUS
Please note: before test should connect LIN BUS including GND, VBAT and LIN. If you test failed, please upload the LIN log captured by PLIN-View Pro.
BR
Tomlin
hello @nxf10035
I am able to generate the log file but in itrc format i am sharing the log file with you but the error remains
sharing the ECU bus tool error snapshot as well
Thanks
Abhishek
Hi, @Asharm11
From your LIN log the ECU-BUS working normally. The UDS message has been sent to LIN BUS. Suggestion you check LIN configuration of ECU side:
1. Baud Rate
2. I/O as LIN feature
3. Debug ECU side received LIN messages or not
4. Hardware connect
BR
Tomlin
Hii @nxf1003
I have checked the baud rate it was 19200 bps
hardware is connected properly
still I am getting the no response error as shown in the attached snapshot
your help would be appreciated
Regards
Abhishek
Hi, @Asharm11
From my side, some suggestion as following:
1. Check hardware LIN(LPUART instance) and software configure is the same or not
2. Baud rate
3. Hardware connect including: LIN, VBAT and GND
4. Check LIN transceiver configuration
4. If above all is correct, you can capture the LPUART RX and TX signals over oscilloscope. If oscilloscope have not anything signals, then the issue might be from hardware. If the RX line have signals, then check the LIN driver RX the data or not. This can set a breakpoint in LIN RX ISR.
BR
Tomlin
Hello @nxf10035,
I updated the ECU bus too to v0.2.24 and now I am getting this error"[4970ms][sch1]{"msg":"No response","index":1}" attaching the snapshot
and could you tell me how you generated the log file
Regards
Abhishek