LIN Communication not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN Communication not working

4,806件の閲覧回数
shravani
Contributor II

Hello

I have configured LIN protocol through configurator on S32DS and checking for the interrupt is coming or not.

I am checking by connecting a CAN analyzer and sending the frame every 10ms to check the interrupt.
I put a breakpoint at ISR. When I try to run the code, interrupt is coming only once. Even though hardware(CAN analyzer is not connected interrupt is coming.

How to solve this issue? Your help is highly appreciated.

Please find below details

Chip Model: S32K312_100MQFP, 

S32DS version: 3.5

SDK: PlatformSDK_S32K3_2022_03

RTD: SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204

AUTOSAR MCAL used: Yes.

 

 

0 件の賞賛
返信
2 返答(返信)

4,745件の閲覧回数
shravani
Contributor II

Hi @cuongnguyenphu,

Thanks for the reply. I will check config and dump registers.

Please check the attached configurations of the LIN driver for your reference.

Note: LPUART0_CLK is 8MHz.

 

 

 

 

 

 

0 件の賞賛
返信

4,754件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
If the interrupt is triggered even though HW is not connected, then you should check your config and dump register to check that what is the event of that interrupt.
I think it's need more detail in your case to check the issue: Register dump, configurations, how did you call functions...
Please give us more information about that to clarify this 

0 件の賞賛
返信