KITFS85SKTEVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KITFS85SKTEVM

1,174 Views
yavuzklc
Contributor I

Hi,

I want to using kıtfs85sktevm board with other mcu(s32k144).I make all configuration that like your documentation.(Connection and software.(FS8x watchdogExample Readme documentation.)).But it is not work.

I see invalid frame (CRC check failed) error on flexgui software.I am beginner what can i do ?

please help me.

Thanks.

Screenshot 2023-02-11 164801.png

 The other  question that i have is, I want to change the voltage value of buck3 using TestMode:MirrorsMain tab. I cannot change the value directly using write button. Changes only applies after disabling and enabling buck3. Is it a normal behaviour ? 

0 Kudos
Reply
1 Reply

1,132 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the response from our specialist below:

Q1: I want to using KITFS85SKTEVM board with other MCU (S32K144).I make all configuration that like your documentation.(Connection and software.(FS8x watchdogExample Readme documentation.)).But it is not work.

I see invalid frame (CRC check failed) error on FLEXGUI software. What can I do ?

1). Make sure that all the steps (FS8x watchdogExample Readme documentation) were done and check the connection quality.

2). Ensure that the two boards are not damaged.

3). Make sure that 12V is applied and wake1 switch is on. 

 

Q2: The other  question that i have is, I want to change the voltage value of buck3 using TestMode:MirrorsMain tab. I cannot change the value directly using write button. Changes only applies after disabling and enabling BUCK3. Is it a normal behavior? 

Online voltage change is not supported for all FS85 regulators. 

Please generate the whole script with correct BUCK3 voltage value and run the FS85 in OTP emulation mode. Please refer to 7.2 in UM11183.  

 

I hope this information helps.

Regards,

David

0 Kudos
Reply