JTAG Access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Access

502 Views
addisonaudette1
Contributor I

I am figuring out how to disable and enable JTAG access on the s32k3x4evb-t172 board and am reading conflicting information. 

In this forum post (Solved: S32 can't find Hardware (S32K344) for Debug - NXP Community) - the solution says There is no on-board programmer/debugger and the S32K344 MCU can be reprogrammed via the J40 JTAG/SWD connector only.

However in the MCU Automotive Board Quick Starts it says you can either connect a micro usb cable to the J4- connector to debug via the on-board s32K3 debugger or just one of the available JTAG connectors to debug via the external S32k3 debugger. 

 

Could someone elaborate which is correct and what the options are for hardware configuration JTAG access?

 

0 Kudos
Reply
1 Reply

485 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @addisonaudette1 

There seems to be some confusion. In the thread you referenced, the discussion is about the S32K3 T-Box, which indeed does not include an on‑board debugger.

However, the S32K3X4EVB‑T172 does include an on‑board debugger, and it also provides an embedded JTAG connector (J12). You can use either of these interfaces to flash and debug the MCU.

 

BR, VaneB

0 Kudos
Reply