Issue with LPUART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with LPUART

2,345件の閲覧回数
pankajprasad100
Contributor III

Hi,

   I am working with S32K116 in which using example code for LPUART.

While checking the signals using oscilloscope i can see highs and lows but the voltage levels are in 250 to 300 mV range.

Well i think voltage levels should be should be in volts not in milli volts.

Any reason behind it?

 

Thanks & Regards

PANKAJ PRASAD

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,338件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Pankaj,

Which LPUART examples do you use?

Do you have an EVB or your custom board?

Which pins do you scope?

The voltage levels depends on the power supply as you can see in the DS, rev.13, Chapter 5, I/O parameters.

 

Regards,

Daniel

0 件の賞賛
返信

2,324件の閲覧回数
pankajprasad100
Contributor III

1.lpuart echo s32k116

2.custom board

3.rx-PTC2   tx-PTC3

 

0 件の賞賛
返信

2,295件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Pankaj,

The issue was reportedly solved.

If not, let me know.

 

Regards,

Daniel

 

0 件の賞賛
返信