Issue with LPUART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with LPUART

2,349 次查看
pankajprasad100
Contributor III

Hi,

   I am working with S32K116 in which using example code for LPUART.

While checking the signals using oscilloscope i can see highs and lows but the voltage levels are in 250 to 300 mV range.

Well i think voltage levels should be should be in volts not in milli volts.

Any reason behind it?

 

Thanks & Regards

PANKAJ PRASAD

标记 (1)
0 项奖励
回复
3 回复数

2,342 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Pankaj,

Which LPUART examples do you use?

Do you have an EVB or your custom board?

Which pins do you scope?

The voltage levels depends on the power supply as you can see in the DS, rev.13, Chapter 5, I/O parameters.

 

Regards,

Daniel

0 项奖励
回复

2,328 次查看
pankajprasad100
Contributor III

1.lpuart echo s32k116

2.custom board

3.rx-PTC2   tx-PTC3

 

0 项奖励
回复

2,299 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Pankaj,

The issue was reportedly solved.

If not, let me know.

 

Regards,

Daniel

 

0 项奖励
回复