Issue Regarding CAN Filter mask.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue Regarding CAN Filter mask.

2,447件の閲覧回数
sandhyaravikuma
Contributor II

Greetings,

I am using NXP arm design studio for s32k144 chip set,

For receiving a specific extended CAN message from a external device I have configured the CAN filter mask, after the filter mask configuration is made I'm receiving configured messages as well as non-configured messages also.

Here i am attaching my configuration, kindly help me to over come this issue.

 

/*! @brief PAL instance information */
const can_instance_t canPal1_instance = {CAN_INST_TYPE_FLEXCAN, 1U};

/*! @brief User configuration structure */
const can_user_config_t canPal1_Config0 = {
.maxBuffNum = 16UL,
.mode = CAN_NORMAL_MODE,
.peClksrc=CAN_CLK_SOURCE_PERIPH,
.enableFD = false,
.payloadSize = CAN_PAYLOAD_SIZE_8,
.nominalBitrate = {
.propSeg = 7,
.phaseSeg1 = 4,
.phaseSeg2 = 1,
.preDivider = 2,
.rJumpwidth = 1
},
.dataBitrate = {
.propSeg = 7,
.phaseSeg1 = 4,
.phaseSeg2 = 1,
.preDivider = 2,
.rJumpwidth = 1
},
.extension = NULL,
};

//Initialisation
unsigned char Can_Init(void)
{
unsigned char ret_val_u8 = 0;

/*#1 Initialize CAN engine - baudrate, DMA or IT, filter buffer init with table */
ret_val_u8 = CAN_Init(&canPal1_instance, &canPal1_Config0);

/*#2 Configure the Tx buffer using MailBox 0 & 1*/
can_buff_tx_config_e.enableFD = FALSE;
can_buff_tx_config_e.enableBRS = FALSE;
can_buff_tx_config_e.idType = CAN_MSG_ID_EXT;
can_buff_tx_config_e.isRemote = FALSE;
can_buff_tx_config_e.fdPadding = 0;

ret_val_u8 += CAN_ConfigTxBuff(&canPal1_instance, TX_MAILBOX0, &can_buff_tx_config_e);
ret_val_u8 += CAN_ConfigTxBuff(&canPal1_instance, TX_MAILBOX1, &can_buff_tx_config_e);

/*#3 Configure the Rx buffer using MailBox 2 */
can_buff_rx_config_e.enableFD = FALSE;
can_buff_rx_config_e.enableBRS = FALSE;
can_buff_rx_config_e.idType = CAN_MSG_ID_EXT;
can_buff_rx_config_e.isRemote = FALSE;
can_buff_rx_config_e.fdPadding = 0;

/*#4 Start reception of Rx Buffer (initially with a fixed acceptance address (NULL)) */
/* NULL is assigned in order to avoid any incoming messages before application starts */
ret_val_u8 += CAN_ConfigRxBuff(&canPal1_instance, RX_MAILBOX0, &can_buff_rx_config_e, MIN_U32);

/*#5 Change the mask mode to "Individual Mask" (so other Masks will be zero) with complete masking */
ret_val_u8 += CAN_SetRxFilter(&canPal1_instance, CAN_MSG_ID_EXT, RX_MAILBOX0, 0);

/*#6 Inclusion of callback function of the IT and DMA events */
/* FlexCAN driver includes few additional functionality than CAN-PAL drivers
* NOTE: Don't use RxFIFO feature in Can_Init if we use this callback */
FLEXCAN_DRV_InstallEventCallback(canPal1_instance.instIdx, Can_Callback_Event, NULL);
return(ret_val_u8);
}

/* #1 Configure the Rx Mailbox with required address */
ret_val_u8 = CAN_ConfigRxBuff(&canPal1_instance, FILTER_BANK_0,&can_buff_rx_config_e, 0x01023345);

/* #2 Configure the Mask of the Rx Mailbox */
ret_val_u8 += CAN_SetRxFilter(&canPal1_instance, CAN_MSG_ID_EXT, FILTER_BANK_0,0x1FFFFFFF);

Thanks,

0 件の賞賛
返信
2 返答(返信)

2,408件の閲覧回数
sandhyaravikuma
Contributor II

Thanks PetrS. This issue is resolved.

Regards

0 件の賞賛
返信

2,430件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

if you clear mask acceptance register then all IDs will be accepted to respective message buffer if it is free to receive.

 

BR, Petr 

0 件の賞賛
返信