Interfacing S32K144 with an external EEPROM using I2C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing S32K144 with an external EEPROM using I2C

7,037件の閲覧回数
Rambo1310
Contributor I

Interfacing EEPROM BR24T512-3AM with S32K144. I have tried to establish the interface by writing a value to a particular address  and then reading it back from the same address.

However I'm getting the status while sending and receiving data over I2C as "STATUS_I2C_RECEIVED_NACK".

PFA the sample code for this task. Kindly review and help sort out the issue.

 

Thanks

0 件の賞賛
返信
6 返答(返信)

7,010件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Rambo1310,

Can you menasure the bus with an oscilloscope?

If there is no ACK, check the address.

 

Thanks,

BR, Daniel

0 件の賞賛
返信

7,000件の閲覧回数
Rambo1310
Contributor I
The 7 bit address is 0x50.
The read/write bit i.e the 8th bit is 0 for writing and 1 for reading.
I have implemented the logic in the respective function.
0 件の賞賛
返信

6,992件の閲覧回数
Rambo1310
Contributor I

The write and read cycle as per datasheet has been attached for your reference. I don't understand where am going wrong with this. Is the I2C peripheral initialized and APIs used correctly?

 

0 件の賞賛
返信

6,985件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

There is no need to initialize the driver and to set the address in every function, do it just once.

The driver changes the R/W bit in the address depending on the LPI2C API used:

LPI2C_DRV_MasterSendDataBlocking()

LPI2C_DRV_MasterReceiveDataBlocking()

Don't change the address using the LPI2C_DRV_MasterSetSlaveAddr() function.

 

It is important to measure the bus using an oscilloscope or a logic analyzer to make sure the signals are correct.

 

Regards,

Daniel

 

 

0 件の賞賛
返信

6,958件の閲覧回数
Rambo1310
Contributor I

I made these changes but didn't work. Same status is returned.

I even tried changing the component to I2C_pal from LPI2C but still no luck am not able to write and read the desired data.

PFA the modified code.

 

0 件の賞賛
返信

6,926件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

I don't see any obvious issue in the code.

As I said, it is necessary to scope the bus, and compare it with the expected signal as per the datasheet of the EEPROM.

 

Regards,

Daniel

0 件の賞賛
返信