ICU S32K116

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICU S32K116

1,044 Views
Ahmed_Attia
Contributor I

"Hello NXP,

I am currently working with the Input Capture Module (ICU). I have configured it in the time stamp mode with a rising edge interrupt. Additionally,

I have set up FTM0 Channel 6. FTM0 is operating at an 8MHz SIRC clock, and I have configured the ICU channel with a prescaler of 128, resulting in a tick time of 16 microseconds.

With this configuration, the ICU channel can measure time intervals ranging from 16 microseconds to 1048560 microseconds, which is equivalent to over 1 second.

It works well with higher frequencies and shorter periods, from 16 microseconds up to 70 milliseconds. However, beyond 70 milliseconds, I encountered an issue where the values obtained include additional pulse ticks, as listed below:

Ahmed_Attia_0-1694108249603.png

 

For 77 milliseconds, I observed a pulse with 3 additional ticks, indicating an error.

For 500 milliseconds (half a second), I observed a pulse with 10 additional ticks, and so on. I am curious if there is a specific reason for this behavior when working with lower frequencies.

Please note that I am using an NXP S32K116 microcontroller and configuring ADC0 using the TRESOS tool with the SW32K1_RTD_4.4_1.0.1_HF01_D2209 package."

0 Kudos
Reply
0 Replies