Hi @Jusaira
The configuration of these signals depends on if it uses I2C in 4-wire mode or 2-wire mode.
For SCLS in "4-wire mode, this is the SCLS output pin. If LPI2C master/slave are configured to use separate pins, then this the LPI2C slave SCL pin."
For SDAS in "4-wire mode, this is the SDAS output pin. If LPI2C master/slave are configured to use
separate pins, then this the LPI2C slave SDA pin."
Please look at Chapter 52 (Low Power Inter-Integrated Circuit (LPI2C)) of the S32K1xx Series Reference Manual, Rev. 13, for more information about this module.
B.R
VaneB