HvBms_CmuBjbSenseMon Integration and User Manuals missing from SDK package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HvBms_CmuBjbSenseMon Integration and User Manuals missing from SDK package

1,144 Views
pjadhav21
Contributor II

Hello Team,

 

We are trying to integrate components from SW32K3_BMS_APP_R21-11_0.8.0. We were able to configure MCAL components for BJB and CMU but application components HvBms_BjbSenseMon, HvBms_CmuSenseMon, HvBms_CmuIf, HvBms_BjbIf are giving us lot of integration as well as compilation errors. 

I will keep posting errors which we are getting in this thread but before that there is no documentation for integrating these components. Integration as well as User manuals are not available for these components. Can you please provide the same please. 

 

Thanks,

Pratik

0 Kudos
Reply
3 Replies

1,115 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @pjadhav21,

According to the release notes of SW32K3 BMS Application AUTOSAR 4.4_R21-11 0.8.0 D2402, you should follow "BMS_SWInstalationGuide_Application.pdf present in package manager". Can you confirm it was installed correctly?

Do you use updatesite.zip package in S32DS IDE, or did you install the standalone .exe version?

There are UM and IM documents:

danielmartynek_0-1748246341586.png

 

Best regards,

Daniel

0 Kudos
Reply

1,097 Views
pjadhav21
Contributor II

Files which are shown in the screenshot which you shared, are for BMS_Common component. There is no information related to CMUsense and BJUsense components. 

pjadhav21_1-1748290424205.png

 



I can confirm I have installed all the packages correctly and using .zip files. 

0 Kudos
Reply

1,052 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @pjadhav21,

You're right — documents are for the BMS_Common driver only.
Following my discussion with the HvBms team, unfortunately, the requested manuals are not available. However, the integration project is available and can be used as a reference.

danielmartynek_0-1748507711646.png

 

 

Regards,

Daniel

 

 

 

0 Kudos
Reply