I want to use sja1110 EVM as a switch, but the sfp of the sja1110 can not work. Does it have some examples that can make the sfp work.
Hi @cuiyunxiao ,
there are example projects in the SJA1110 SDK which configure the board infrastructure accodingly. The SFP modules should then also be working. Please note that one SFP is connected to switch-1 and the other two SFPs are connected to switch-2 on the board.
Please note that all SFPs use SGMII interface. Which SFP slots do you use for the cages?
Please refer also to the SJA1110-EVM user manual for further explanation.
BR
Kevin