How to make Enhanced FIFO only receive extended ID message with s32k3.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make Enhanced FIFO only receive extended ID message with s32k3.

2,611 Views
luhaiou
Contributor II

The S32K3 reference manual mentioned the enhanced FIFO can receive 2 different CAN message types.

But now I only want to receive one type message----extended ID message.

luhaiou_0-1735291058011.jpeg

If I set the standard ID filter elements  to 0,(i.e. NEXIF == NFE+1)

whether all standard ID messages can be blocked

0 Kudos
Reply
5 Replies

2,590 Views
IsaulO
NXP Employee
NXP Employee

Hi @luhaiou ,
NFE defines the total number of filter elements used during the enhanced RX FIFO matching process and NEXIF defines the number of extended ID filter elements used during the Enhanced RX FIFO matching process.
The relationship between NEXIF and NFE:

IsaulO_0-1735326727877.png

If you want to receive Extended ID format, you can specify this in the IDE field (Table 524.Field descriptions of reference manual), this Identifies whether the frame format is standard or extended.
1: Frame format is extended
0: Frame format is standard

In standard frame format, only the 11 most significant bits (28 to 18) are used for frame identification in both receive and transmit cases. The 18 least significant bits are ignored. In extended frame format, all bits are used for frame identification in both receive and transmit cases.

For more detailed information about Message buffer structure and Enhanced RX FIFO matching process, please refer to the latest version of the Reference Manual:
S32K3xx MCU Family - Reference Manual

Hope it helps you.

BR,

IsaulO.

0 Kudos
Reply

2,556 Views
luhaiou
Contributor II

Thank you very much for your reply.

For enhanced RX FIFO Filter element, there is no IDE bit to set, 

luhaiou_1-1735524107884.png

Now I want to implement filtering all standard IDs.

when Enhanced RX FIFO matching process,

how to confirm the filter element is for  extended ID or standard ID

For enhanced FIFO, there are 128 Filter element.

When the matching process starts, does it always start with the first filter element?

For example,
I set  NFE=0, NEXIF =1.There is no standard ID filter element at this point.

Now controller receives a standard ID frame message.

At this time, there is no standard id filter element, so does the controller still have to try to match the processing.

If it try to match the processing, there is no IDE bit in the filter element,

then how can the filter element of the extended ID message match the standard ID message

I'd like to know the detailed steps in this scenario?

Thank you very much

 

0 Kudos
Reply

2,498 Views
IsaulO
NXP Employee
NXP Employee

This process is explained in detail in the 73.3.8.1 Enhanced RX FIFO matching process chapter of the Reference Manual.

Depending on the filter scheme, the matching process may vary, but the first matching criteria for any ID filter scheme is to verify the CAN Message ID type.
CAN message is extended frame format (IDE = 1).
CAN message is base frame format (IDE = 0).

If at least one filter element satisfies the matching criteria, the CAN message content is transferred to the enhanced RX FIFO memory.


Additionally, you can consult this example regarding Enhanced FIFO usage:
Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200 - NXP Community

BR,

IsaulO

0 Kudos
Reply

2,484 Views
luhaiou
Contributor II

Thank you very much for your reply.

I have read the reference manual,The introduction is not detailed enough,

you can judge the type of frame through the IDE BIT,

but there is no IDE BIT in the RX FIFO Filter element,

so how to determine whether this RX FIFO Filter element is an extended frame Filter or a standard frame Filter?

For example,
I set  NFE=0, NEXIF =1.There is no standard ID filter element at this point.

Now controller receives a standard ID frame message.

At this time, there is no standard id filter element, so does the controller still have to try to match the processing.

If it try to match the processing, there is no IDE bit in the filter element,

then how can the filter element of the extended ID message match the standard ID message

I'd like to know the detailed steps in this scenario?

Thank you very much

0 Kudos
Reply

2,426 Views
IsaulO
NXP Employee
NXP Employee

Hi @luhaiou , 


The filter memory space can be split into two regions: one for extended-ID filter elements and another for standard-ID filter elements, according to ERFCR[NEXIF].

IsaulO_0-1736276377657.png

 

If we consider your configurations (NFE=0, NEXIF=1), the controller will search for a match with an Extended CAN Message by scanning the first region for extended-ID filter elements. The filter configurations should be specified in the first pair of ERFFEL registers.


You can check the following demo application for more information regarding Enhanced RX FIFO.
Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMA test S32DS3.5 RTD400 - NXP Community


BR,
IsaulO.

 

0 Kudos
Reply