How to generate the S32K144 + FREERTOS project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate the S32K144 + FREERTOS project

1,505件の閲覧回数
rupingliu
Contributor I

I want to know how to create S32K144+freertos project in S32 Design Studio V3.5.

thank you!

0 件の賞賛
返信
1 返信

1,483件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @rupingliu 

After the project with the SDK is created and the configuration opened, SDK components can be added to the project. For this you have tow ways to do it:
1- Right click on the project, choose “S32 Configuration Tools”, and then “Manage SDK Components"

VaneB_0-1666293069701.png

2- Select project, click on “S32 Configuration Tools” icon on the upper toolbar,and then “Manage SDK Components"

VaneB_1-1666293127146.png

After the option is selected, a dialog with the supported components for the SDK project SDK is displayed:

VaneB_2-1666293204168.png

 

Available options that can be chosen are:

  • Copy sources -> If checked, sources are copied to the workspace project, otherwise they are linked from existing sources in the SDK.
  • Import other files -> If checked, other files listed in the SDK components and/or example.xml will be imported.
  • Sync with Peripherals Tool Configuration view, automatic add/remove components -> If true, for each dependency, if available, in Peripherals Tool Configuration the drivers will be added/removed only if the configuration for the selected project is opened.

After the components are selected/unselected, and “OK” button is pressed, a pop-up with all the drivers sources will be displayed for each operation: add to project or remove from project:

VaneB_3-1666293494738.png

 

I hope this will help you.

B.R.

VaneB

0 件の賞賛
返信