How to find the S32K3xx FreeRTOS TCP/IP stack driver and example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to find the S32K3xx FreeRTOS TCP/IP stack driver and example

6,278 Views
cranes
Contributor IV

Hello,

Is there valid S32K3xx FreeRTOS TCP/IP stack driver and example available?

I downloaded all below installations and still failed to install any one of them.

cranes_0-1701657828792.png

There is a post https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052 talking about this issue. But both two files mentioned in the post  S32K396_updatesize.zip and SW32K396_S32DS_3.5.1_D2207.zip can't be found any more.

Thanks!

Crane

 

0 Kudos
Reply
10 Replies

6,261 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try this link; https://nxp.flexnetoperations.com/control/frse/download?element=13661857

Or go through Automotive SW - S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio -> click to Previous tab -> find S32 Design Studio Service Pack 1 EAR 1 with support for S32K396 devices 

BR, Petr

0 Kudos
Reply

6,244 Views
cranes
Contributor IV

Thanks PetrS!

I do find the file and installed the S32K396 development package and RTD ver 3.0.0 successfully.

But how to find the TCP/IP stack? Checked the example available, and found two ethernet loopback examples. Is it in there?

Thanks!

Crane 

0 Kudos
Reply

6,231 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check installation folder, if it really includes this stack. Examples are there...

PetrS_0-1701848785895.png

you can create new project from example within S32DS

PetrS_1-1701848930504.png

BR, Petr

0 Kudos
Reply

6,213 Views
cranes
Contributor IV

Hello PetrS,

This is what I see in my folder after installing SW32K396_S32DS_3.5.1_D2207.zip:

cranes_0-1701915511876.png

In the PlatformSDK_S32K3 folder, only RTD, there is no stack folder.

These are what's installed:

cranes_1-1701915842680.png

When creating the project from the example, only RTD, no TCP/IP stack.

Anything might be missed in my installation?

Regards,

Crane

 

0 Kudos
Reply

6,206 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

so if you now add/install tcpip stack, will it pass without any error popped out and appears within install folder?

BR, Petr

0 Kudos
Reply

6,188 Views
cranes
Contributor IV

Hi PetrS,

Only S32K396_TCPIP_RTM_1_0_2_CD01_D2208_updatesite.zip adds it to the available software. And it requires FreeRTOS. 

When installing SW32K396_FreeRTOS_10_4_6_UOS_0_8_0_DS_updatesite_D2208.zip, I got this error:

cranes_0-1701995960925.png

But RTD S32K3xx v3.0.0 is already installed.

cranes_2-1701996066628.png

What might be still missing?

Thanks!

Crane

 

0 Kudos
Reply

6,086 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the FreeRTOS for S32K396 requires particular version of RTD. Based on FreeRTOS for S32K396 release notes the required RTD version is Code Drop 02 and S32K396 dev package EAR2:

jiri_kral_0-1702901181045.png

With this configuration you should be able install FreeRTOS package. 

0 Kudos
Reply

6,082 Views
cranes
Contributor IV

Hello,

Ok got it. Thank you!

For RTD, I can only find these versions and couldn't find the version mentioned in your reply.

cranes_0-1702924120265.png

cranes_2-1702924387903.png

cranes_1-1702924327076.png

It happened before with another file as described in my another post. Is there anything missing in my searching or it indeed doesn't exist any more?

Thanks!

Crane

0 Kudos
Reply

6,073 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to check "Previous" tab as well

PetrS_0-1702987349745.png

BR, Petr

0 Kudos
Reply

6,067 Views
cranes
Contributor IV

Hello,

This is really weird. This is what I see in the previous tab:

cranes_0-1703000125361.png

Thanks!

Crane

 

0 Kudos
Reply