How to disable FlexCAN auto re-transmitting feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable FlexCAN auto re-transmitting feature

813件の閲覧回数
YuhuiMa
NXP Employee
NXP Employee

Hi, 

My goal is to let FlexCAN always only send single-shot CAN message.

I am currently using S32K144 SDK to play with FlexCAN.

The current situation is, when a CAN message was not acknowledged by any receiver or any error was reported, the FlexCAN will repeatedly re-transmit this CAN message until it's ACKed or timeout.

For some CAN messages, I just want FlexCAN to send message frame only once without any re-transmitting. Where is that magic reg/bits?

Plus, much appreciate if you could provide an example code on that. (I am just new to S32K)

Thanks

0 件の賞賛
返信
1 返信

806件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Yuhui,

there's no such option, this behavior is given by CAN spec.

Solution is to connect another node which will acknowledge the message.

Or, if it is for test purposes only, you can use internal loop back mode (LPB bit in CTRL1 register). In this mode, you will receive what you sent and ACK is ignored.

Regards,

Lukas

 

 

0 件の賞賛
返信