How to configure the MC33771C for 7 cells

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure the MC33771C for 7 cells

ソリューションへジャンプ
2,515件の閲覧回数
Zyuan17
Contributor III

I am current use 7 cells to test the board. I have successfully monitor the voltage and current. But the fault register has a problem. I have configured the overvoltage threshold and undervoltage threshold to 2800mV and 4200mV. drvCfg:

drvConfig.drvInstance = 0U;
drvConfig.commMode = BCC_MODE_SPI;
drvConfig.devicesCnt = 1U;
drvConfig.device[0] = BCC_DEVICE_MC33771C;
drvConfig.cellCnt[0] = 7U;
drvConfig.loopBack = false;

But when I check the registers, the fault register for 5 to 11 cells are undervoltage. How should I solve this?

Codes for reading the fault registers:

error = BCC_Fault_GetStatus(&drvConfig, BCC_CID_DEV1, faultStatus);
if (error != BCC_STATUS_SUCCESS)
{
return error;
}

faultStatusValue[0] = faultStatus[BCC_FS_CELL_OV];
faultStatusValue[1] = faultStatus[BCC_FS_CELL_UV];

return BCC_STATUS_SUCCESS;

 

 

 

0 件の賞賛
返信
1 解決策
2,492件の閲覧回数
Zyuan17
Contributor III

I have found a solution, I disabled the cell 5 to 11 fault detection.

 

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT14_OFFSET, MC33771C_TH_CT14_CT_UV_TH_MASK, MC33771C_TH_CT14_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT13_OFFSET, MC33771C_TH_CT13_CT_UV_TH_MASK, MC33771C_TH_CT13_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT12_OFFSET, MC33771C_TH_CT12_CT_UV_TH_MASK, MC33771C_TH_CT12_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT11_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT11_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT10_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT10_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT9_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT9_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT8_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT8_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT7_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT7_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT6_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT6_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT5_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT5_OVUV_EN_DISABLED_ENUM_VAL);

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT4_OFFSET, MC33771C_TH_CT4_CT_UV_TH_MASK, MC33771C_TH_CT4_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT3_OFFSET, MC33771C_TH_CT3_CT_UV_TH_MASK, MC33771C_TH_CT3_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT2_OFFSET, MC33771C_TH_CT2_CT_UV_TH_MASK, MC33771C_TH_CT2_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT1_OFFSET, MC33771C_TH_CT1_CT_UV_TH_MASK, MC33771C_TH_CT1_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,493件の閲覧回数
Zyuan17
Contributor III

I have found a solution, I disabled the cell 5 to 11 fault detection.

 

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT14_OFFSET, MC33771C_TH_CT14_CT_UV_TH_MASK, MC33771C_TH_CT14_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT13_OFFSET, MC33771C_TH_CT13_CT_UV_TH_MASK, MC33771C_TH_CT13_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT12_OFFSET, MC33771C_TH_CT12_CT_UV_TH_MASK, MC33771C_TH_CT12_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT11_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT11_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT10_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT10_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT9_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT9_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT8_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT8_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT7_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT7_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT6_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT6_OVUV_EN_DISABLED_ENUM_VAL);
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_OV_UV_EN_OFFSET, MC33771C_OV_UV_EN_CT5_OVUV_EN_MASK, MC33771C_OV_UV_EN_CT5_OVUV_EN_DISABLED_ENUM_VAL);

error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT4_OFFSET, MC33771C_TH_CT4_CT_UV_TH_MASK, MC33771C_TH_CT4_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT3_OFFSET, MC33771C_TH_CT3_CT_UV_TH_MASK, MC33771C_TH_CT3_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT2_OFFSET, MC33771C_TH_CT2_CT_UV_TH_MASK, MC33771C_TH_CT2_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));
error = BCC_Reg_Update(&drvConfig, BCC_CID_DEV1, MC33771C_TH_CT1_OFFSET, MC33771C_TH_CT1_CT_UV_TH_MASK, MC33771C_TH_CT1_CT_UV_TH(BCC_GET_TH_CTX((int32_t)MC33771C_TH_ALL_CT_UV_TH)));

 

0 件の賞賛
返信
2,505件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

How did you connect with 7 cells? what part number do you use? MC33771 or MC33772?

 

0 件の賞賛
返信
2,503件の閲覧回数
Zyuan17
Contributor III

I use MC33771C, and short the 5 to 11th cell.

0 件の賞賛
返信
2,499件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can't directly short 5-11 cells, firstly you can configure and test using full 14 cells ,if no more issue please let me know!

0 件の賞賛
返信
2,494件の閲覧回数
Zyuan17
Contributor III
I connect the CT5 to 11 to the negative side of cell 12 and connect the positive side of cell 4 to negative side of cell 12.
0 件の賞賛
返信
2,495件の閲覧回数
Zyuan17
Contributor III
Why I cannot directly short the cells? I have checked the datasheet, I am using FRDM33771CSPEVB. It shows that the 5 to 11 cells can be replaced with dummy cells or shorted. And I have to use 7 cells for my project. I have test the 14-cell setting with lead acid batteries and it works. But I need to change to 7 cells to test the lithium-ion batteries
0 件の賞賛
返信