How to close CAN TX interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to close CAN TX interrupt?

1,838 Views
eautopower
Contributor IV

NOW,i open the CAN interrupt,CAN TX interrupt also open,i want to know how to close the CAN TX interrupt.

0 Kudos
Reply
1 Reply

1,533 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The Message Buffer interrupt is enabled if respective bit in IMASK1 register is set. Then if flag is set in the IFLAG1 register the interrupt is called. The flag is cleared by writing 1 to respective bit in the IFLAG1.

If you do not want to have interrupt generated after successful message transmission, then clear respective bit in IMASK1 register.

BR, Petr

0 Kudos
Reply