How to build a S32k project with makefile

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build a S32k project with makefile

4,313 次查看
xiaomu
Contributor II

I want to learn how to build a S32K project with makefile,so i choose the example project from S32DS stidio.and I can finish the project by normal build way.

But when I change to makefile way,this project complied error.Here's how I did it 。

1:choose the "makefile project with existing code ",and I create a project name ,and find the example project exist.

2:Right click on the project,and enter the properties config sheet.

3:There are 3 config sheets below the C/C++ BUILD .I config the "Behavior"sheet.and I added "allsub"in the build line,and added "clean"in the clean line;like  attachment 1

4: Then I build the project,and the makefile make a error"make: *** No rule to make target 'allsub'. Stop".like attachement 2

5:when  I leave  the build line blank,the makefile also make a error"make: *** No targets specified and no makefile found. Stop."like attachment 3.

How could I slove the probelm?

标记 (1)
0 项奖励
回复
2 回复数

3,823 次查看
luhaiou
Contributor II

Our project will use IAR as the compiler for s32k312.

Can NXP provide a makefile sample project based on IAR toolchain for s32k312.

Looking forward to your reply, thank you very much

0 项奖励
回复

4,296 次查看
Senlent
NXP TechSupport
NXP TechSupport
0 项奖励
回复