How can I let the CAN enter Stop Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I let the CAN enter Stop Mode

1,511件の閲覧回数
春华张
Contributor I

   as the S32Kxx-RM description,the CAN enter the Stop mode,the first step is enter Freeze mode ,and then Stop mode is requested at chip level.

Is there the "chip level Stop" mean "CPU Stop"?If yes,then cpu stop ,how I can know whether the CAN had enter Stop mode?

 Is there have a exmple for CAN stop and wakeup? thanks!

0 件の賞賛
返信
1 返信

1,388件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
Yes, the chip level stop is entered once WFI instruction is executed.
“If FlexCAN receives the global Stop mode request during Freeze mode, it sets the LPMACK bit, negates the FRZACK bit and then sends the Stop Acknowledge signal to the CPU, in order to shut down the clocks globally.” (Section 53.5.11.3 RM rev.9). Please see Section 25.2.2.6 Stop mode acknowledge error.

Regards,
Daniel

0 件の賞賛
返信