Hard Fault in ImportPlainSymKeyReq() when running SecureBootAppNoteDemo on S32K344EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard Fault in ImportPlainSymKeyReq() when running SecureBootAppNoteDemo on S32K344EVB

1,575 Views
Luu_Nghia_308
Contributor II

Dear NXP Support Team,

I am currently trying to run the sw745310 SecureBootAppNoteDemo with AB Swap on the S32K344EVB-T172 board.

During execution, I encounter a Hard Fault when the application calls the function ImportPlainSymKeyReq().

Luu_Nghia_308_0-1767774242446.png

 

Could you please help me analyze what might be causing this issue or suggest how to debug it further?

Thank you very much for your support.

0 Kudos
Reply
4 Replies

1,543 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Have you followed procedure as described in readme.txt file, step by step? It is needed to built App project first then Cfg

0 Kudos
Reply

1,494 Views
Luu_Nghia_308
Contributor II

Hi @davidtosenovjan 

To be compatible with the S32K344 EVB board, I reconfigured the corresponding pins.
I changed the package from BGA 257 to MQFP 172.
I rebuilt the application code first, then rebuilt the configuration (cfg) code.
I also observed that some logs were printed via UART.
From the call stack, can you point out which part looks abnormal?

Luu_Nghia_308_2-1767860367237.png

 

Luu_Nghia_308_1-1767860308365.png

 

Luu_Nghia_308_0-1767859943571.png

 

0 Kudos
Reply

1,320 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am apologizing, I was out of office for couple of days.

Is there any progress on your side?

Are you using the same S32DS and RTD versions as specified?

Unfortunately this appnote is a bit outdated in comparsion to current RTD releases.

Secure boot is also covered in HSE demo examples

davidtosenovjan_0-1768315785629.png

 

0 Kudos
Reply

1,280 Views
Luu_Nghia_308
Contributor II

Hi @davidtosenovjan 

Currently, I am trying to develop based on the HSE example. You may close this ticket and assist me through the following ticket instead:

https://community.nxp.com/t5/S32K/Issue-with-FLASH-Write-Not-Programming-CMAC-Tag-in-S32K344/m-p/229...

 
Thank you very much.
0 Kudos
Reply