Handling power failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Handling power failure

2,451件の閲覧回数
ummerkunnummalk
Contributor III

Hello,

        We use s32k148 in our project and would like to know the failsafe mechanism available in the following scenario:

We need to update the application start adress by modifying vector table at 0x0000_0000.

For this we have erased the first sector from 0x0000_0000 using FTFC commands  and then before programming it with the new address a power failure has occurred.

What will be the behavior in this case once the power is up again?

And is there any mechanism to handle this situation?

Regards,

Ummer K

2 返答(返信)

2,342件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Ummer,
There is no safe mechanism. Such an interruption of an erase or program command can lead to corruption of the flash content. Please note that the first sector 4KB (0x1000) includes not only the vector table but the Flash configuration field (Section 36.4.1, RM rev9) as well.

Regards,
Daniel

2,342件の閲覧回数
ummerkunnummalk
Contributor III

Thanks Daniel for the update.

0 件の賞賛
返信