HSE firmware installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE firmware installation

38,783 Views
vikmonti7804
Contributor III

Hi,

     I want to install the HSE firmware, but i am facing one error with the package given C:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_HSE_FW_INSTALL.

error

make: *** [makefile:38: S32K312_HSE_FW_INSTALL.elf] Error 1

Kindly let me know the solution.

is there any firmware available for s32k312 for HSE fw installation?

0 Kudos
Reply
45 Replies

9,671 Views
Sanjana_k
Contributor II

Hello guys are you able to solve the error.If yes please help us with this 

0 Kudos
Reply

10,901 Views
anakha
Contributor III

Does someone solve the problem? 

I am issuing same steps with you. I tried both full_mem and ab_swap. both failed..

 

0 Kudos
Reply

21,484 Views
sandor_b
Contributor II

Hi,

The "3.3.1 MU Installation steps by host in AB_SWAP configuration" chapter of HSE_B Firmware Reference Manual starts by the following lines:

"Write 0xA5 on register DCMRWP1 (0x402AC400, [24:31 bits]) followed by functional reset. This will set Bit 1 in HSE GPR (0x4039C028) indicating SBAF has activated MU0 for installation."

but it wasn't mentioned in this thread.

Is it necessary to set DCMRWP1 register or is it implemented somehow in the example?

Regards,
Sandor

0 Kudos
Reply

21,985 Views
zkah
Contributor I

Hi,

Has the problem been solved? What causes this? My side is also the status register can not be set "1", can you share how to solve?

0 Kudos
Reply

21,439 Views
sandor_b
Contributor II

Hi,


I think I found a solution. In the memory view, the byte order will be reversed if you select "Hex" or "Hex Integer". The register was set for me, but these views confused me.

 

0 Kudos
Reply

26,057 Views
vikmonti7804
Contributor III

Hi Lucas,

           Can you please share your main program.

i have only one board with me and its new one.

0 Kudos
Reply

26,047 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Attached is whole project.

0 Kudos
Reply

26,515 Views
vikmonti7804
Contributor III

HI,

  the Firmware for the s32k312 is only the file like interface and host, it is not complete project which can flash the HSE firmware binary to controller like s32k344 hse demo example.

I am facing a issue to flash the HSE firmware binry to cntroller as NXP provided only .bin file, i have used the PE micro and eval board built in debugger which is unable to do so, it can support only .elf and .hex file. kindly help me to flash the .bin to controller.

0 Kudos
Reply

26,504 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

The firmware is provided in encrypted form as a binary file. Yes, HSE FW installation package contains only the binary (pink) file and corresponding API headers.

For Lauterbach users, there's also HSE DEMOAPP which helps to install the firmware and examine HSE features:

lukaszadrapa_0-1708065109693.pnglukaszadrapa_0-1708065109693.png

But notice that the demo works with Lauterbach debugger only. It won't work with Pemicro.

As you can read in the mentioned application note or in HSE FW RM, the firmware can be installed with or without IVT.

Installation without IVT is easier but you need a tool which is able to load raw binary file to the flash which is not the case of Pemicro debugger. In this case, "with IVT" method is more convenient.

We do not provide S32K344_HSE_FW_INSTALL for each derivative. This is just an example showing how it can be done and it's up to users to create own solution (each customer has different requirements and production tools/capabilities).

What to do:
You can create new application project directly for S32K312 in S32 Design Studio. Then copy the source files from S32K344_HSE_FW_INSTALL, update HseFwHeader_StartAddress in boot_header.c. Then modify the linker file - use linker file from S32K344_HSE_FW_INSTALL as a template. If you read the readme.md file as I suggested earlier, there must be a link to the bin/pink file, so it is linked to the project.

Then, the code will only enable HSE feature flag by programming any value different from 0xFFFFFFFFFFFFFFFF at address 0x1B000000. Then all the conditions for installation are satisfied - HSE feature flag is enabled, IVT points to valid pink image in flash, so SBAF will install the firmware after next reset.

Regards,
Lukas

0 Kudos
Reply

26,410 Views
vikmonti7804
Contributor III

Hi ,

  If I am able to install the HSE firmware successfully, how to verify this firmware is installed in the secure memory correctly or successfully in the memory.

please let me know any method or check the memory?

Thank You

0 Kudos
Reply

26,406 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

You can check bit 0 in HSE GPR status register at 0x4039C028. If it is '1', it means that "HSE FW is present and SBAF Booted HSE Firmware".

You can find this in HSE_B Firmware Reference Manual rev 2.2.

Regards,

Lukas

0 Kudos
Reply

26,373 Views
vikmonti7804
Contributor III

Hi Lucas , 

         I am not able to see this register in any peripheral window in S32DS, Can you please tell me exactly where i can see.

i can see the value 0xC1010000 at 0x4039C028 address.

 

0 Kudos
Reply

26,361 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I don't think the HSE GPR is defined in peripheral structure, so it's necessary to check the memory directly. If you can see 0xC1010000 at 0x4039C028, the HSE FW is obviously not installed.

Is the HSE feature flash at 0x1B000000 programmed?

And one more thing - I can remember that that if you use "without IVT" method to install the firmware, there can't be valid IVT in the flash. Otherwise it does not work. If you loaded the pink/bin file together with some project, it's necessary to remove the IVT. Or "with IVT" method must be used.

Regards,

Lukas

0 Kudos
Reply

26,354 Views
vikmonti7804
Contributor III

Hi,

     I am just following the example code given for the s32k344, so i created same project for the s32k312 and imported the binary from the linker file, i see the 0xAABBCCDD  at 0x1B000000 location in memory window, what can be the problem. Every thing is same as per the example code as s32k344, only i changed the memory location in linker file. Can you please help on urgent basis, or can we connect online for debugging purpose on small call.

please find the snippet of the linker file and program.

vikmonti7804_0-1708531086237.pngvikmonti7804_0-1708531086237.pngvikmonti7804_1-1708531115954.pngvikmonti7804_1-1708531115954.pngvikmonti7804_2-1708531147534.pngvikmonti7804_2-1708531147534.png

 

0 Kudos
Reply

8,962 Views
Sanjana_k
Contributor II

#hello@vikmonti7804  did u get the solution for the above problem that is programm getting stuck at below ..please hep us 

 

 Sanjana_k_0-1764857943379.pngSanjana_k_0-1764857943379.png

if yes please please help us we are trying alot still we are not getting what to do ?

Thank u

0 Kudos
Reply

26,308 Views
vikmonti7804
Contributor III

Hi,

          kindly check the image attached, the header of the AB_Swap is also there in the memory so it means the firmware is flashed in the memory, the utest area has value AABBCCDDDDCCBBAA it means utest is enabled, the HSE GPR register bit 0 is not getting set, i dont know why? it means after reset the SBAF is not installing the hse firmware in secure memory region.

kindly help on urgent basis.

vikmonti7804_0-1708596640252.pngvikmonti7804_0-1708596640252.png

 

 

Tags (1)
0 Kudos
Reply

26,304 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @vikmonti7804 

could you please share that project? I will test it on my side.

Thanks,

Lukas

0 Kudos
Reply

26,298 Views
vikmonti7804
Contributor III

Please find the project.

0 Kudos
Reply

26,206 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Small problem on my side - I found that I already have firmware 2.6.0 on both my boards and it can't be erased (this feature was added in version 2.40.0). I will get brand new board on Monday and I will test it.

I checked the project anyway and I can see nothing wrong. I would just not program the HSE feature flag unconditionally after each reset.

I will let you know the results of my test on Monday.

Regards,

Lukas

0 Kudos
Reply

26,115 Views
vikmonti7804
Contributor III

Hi Lucas

   Any update on this?

Tags (1)
0 Kudos
Reply