hello everyone:
The app I downloaded from the NXP website,However, there was an error while making the compilation.And I have not modified any files.Do you know how to solve it.
Hi @shuaiguo
which version of the demo app is that exactly? And which version of S32 Design Studio did you use? I tested several versions of the demo app in the past and I had no problem. It's just necessary to copy "hse" and "interface" folder as described in the readme file. The readme file also shows which version of S32DS should be used.
Regards,
Lukas
hello @lukaszadrapa :
S32 Design Studio for S32 Platform 3.4
S32K3XX HSE Firmware 0.2.6.0
The MCU I use is the S32K312
I used this version two weeks ago and it worked as expected. Did you follow all the steps described in "4. Setup" section in the readme file? Could you please double check?
Regards,
Lukas
The compilation passed, but the problem is not simulation.Other projects can be simulated
This demo application is built to be used with:
1. S32 Design Studio and Trace32
or
2. Multi GHS and Trace32
The demo application is then loaded and all the operations are started using this custom menu in Trace32:
It's not supposed to be used with Jlink.
Regards,
Lukas