HSE_SRV_RSP_GENERAL_ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HSE_SRV_RSP_GENERAL_ERROR

910件の閲覧回数
Lixinyu
Contributor I

I tried to request SHA256 hash calculation using the HSE module in the S32K312. With the RTD 3.0 package, I encountered the error code HSE_SRV_RSP_GENERAL_ERROR, but when using RTD version 2.0.3, there is no error, and the hash is correctly calculated.

Some details are as follows:

  • HSE version: HSE_FW_S32K3XX_0_2_6_0
  • RTD version: SW32K3_RTD_R21-11_3.0.0_P07_D2306
0 件の賞賛
返信
1 返信

871件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lixinyu 

The most common reason for this error is data cache memory. Are you sure that all the data objects used for communication with HSE are forced to non-cacheable memory? Or did you try to simply disable the data cache completely to see if it makes a difference?

Regards,

Lukas

0 件の賞賛
返信