HSE FW API integration for S32K324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE FW API integration for S32K324

999 Views
anilsp31PA
Contributor III

We want to run our application on the board where HSE-FW is installed.

Our app is working fine without HSE-FW installed. But after installing HSE-FW we are getting debugger error and it goes into Hard Fault. We want to know what needs to be done in our application to run when HSE_FW is installed on the MCU.

Please share reference to any document or links for information on this.

 

Thanks,

Anil

0 Kudos
Reply
2 Replies

989 Views
john_floros
NXP Employee
NXP Employee

Hello,

Please provide the HSE version installed and how it was installed?  Which RTD version are you using?

Are you able to connect with the debugger out of reset so that we can see some registers and determine the reset for the fault.

Regards,

John

0 Kudos
Reply

983 Views
anilsp31PA
Contributor III

I have installed HSE FW "HSE_FW_S32K3XX_0_2_1_0".

RTD Version: 4.0.0.202401161212

After loading the App, we see failure screen with exception details. PFA screenshot for the same.

Regards,

Anil

0 Kudos
Reply