For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar

1,129 Views
SivaB
Contributor III

suggest the correct SDK, GCC tool chain & RTD version for S32K144 to use LIN communication.

1) S32DS 3.4 / 3.5 

2) RTD SW32K1_RTD_4_4_1_0_1_D2202 / S32SDK_S32K1XX_RTM_4.0.3

3) LIN Stack 1.0.1 / 1.0.2

4) DRV driver / IP driver

0 Kudos
Reply
1 Reply

1,121 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@SivaB

Users can understand some differences between RTD and RTM versions from this answer

https://community.nxp.com/t5/S32K/difference-between-s32k1-sdk-and-s32k1-rtd/m-p/1637711#M22289 

For applications developed by non-autosar, I personally prefer to use the RTM version, because the RTM SDK will be more concise. If you use the RTM SDK version, you can only use S32 DS V3.4, GCC V6.3.1

Use RTD to develop Non-Autosar applications, you can try to use the latest S32 DS V3.5, please use the same LIN Stack as the RTD version

0 Kudos
Reply