Flexio_spi_ip_fault in s32k344 lpspi_flexio_ip_transfer_s32k344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flexio_spi_ip_fault in s32k344 lpspi_flexio_ip_transfer_s32k344

跳至解决方案
1,495 次查看
lluo
Contributor III

Hi,

I am trying to run the demo project lpspi_flexio_ip_transfer_s32k344 on S32K3X4EVB-Q257 . I didn't make any change. As for the hardware connection, I followed the instruction as shown in the description.txt file. 

The code got stuck in the following line:

while (FLEXIO_SPI_IP_IDLE != Flexio_Spi_Ip_GetStatus(SLAVE_EXTERNAL_DEVICE.Instance));

I found there was a fault called Flexio_spi_ip_fault happens as shown in the attached image. Do you probably know why this happens? 

 

Thank you in advance.

0 项奖励
回复
1 解答
1,423 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

If you encounter the problem again, please tell me how to reproduce the problem so that I can test and check the cause.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,468 次查看
SParihar
Contributor III

I am also having same issue when I configure 2 FlexIOs to for SPI communication similar to the example lpspi_flexio_ip_transfer_s32k344. I am using the s32k3x4evb q172 board and have followed the instruction provided in description.txt

I also faced issues in running the SPI transfer example which has not been solved yet,
https://community.nxp.com/t5/S32K/Lpspi-Flexio-Ip-Transfer-S32k344-SPI-example-is-not-working/m-p/17...

0 项奖励
回复
1,415 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

My colleague will communicate with you in your post. 

0 项奖励
回复
1,480 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Which version of S32K3 RTD are you testing?

Since you are using S32K3X4EVB-Q257, do you use Pinmatrix to connect the SPI pins as mentioned in description.txt?

Lpspi_Flexio_Ip_Transfer_S32K344_RTD300P07 description.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,472 次查看
lluo
Contributor III

Hi, Robin,

Thank you for your reply. We soldered extra wires on the board as shown in the circled area in the attached screenshot. And I am using s32 design studio 3.5. The S32K RTD  that I am using is RTD 4.0.0 D2311. Today I've tried to run the demo and it is working, though I still have no idea why the fault happened yesterday.  

0 项奖励
回复
1,424 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

If you encounter the problem again, please tell me how to reproduce the problem so that I can test and check the cause.

0 项奖励
回复
1,421 次查看
lluo
Contributor III

noted. Thank you.

0 项奖励
回复