Flexio_spi_ip_fault in s32k344 lpspi_flexio_ip_transfer_s32k344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexio_spi_ip_fault in s32k344 lpspi_flexio_ip_transfer_s32k344

Jump to solution
1,141 Views
lluo
Contributor III

Hi,

I am trying to run the demo project lpspi_flexio_ip_transfer_s32k344 on S32K3X4EVB-Q257 . I didn't make any change. As for the hardware connection, I followed the instruction as shown in the description.txt file. 

The code got stuck in the following line:

while (FLEXIO_SPI_IP_IDLE != Flexio_Spi_Ip_GetStatus(SLAVE_EXTERNAL_DEVICE.Instance));

I found there was a fault called Flexio_spi_ip_fault happens as shown in the attached image. Do you probably know why this happens? 

 

Thank you in advance.

0 Kudos
Reply
1 Solution
1,069 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

If you encounter the problem again, please tell me how to reproduce the problem so that I can test and check the cause.

View solution in original post

0 Kudos
Reply
6 Replies
1,114 Views
SParihar
Contributor III

I am also having same issue when I configure 2 FlexIOs to for SPI communication similar to the example lpspi_flexio_ip_transfer_s32k344. I am using the s32k3x4evb q172 board and have followed the instruction provided in description.txt

I also faced issues in running the SPI transfer example which has not been solved yet,
https://community.nxp.com/t5/S32K/Lpspi-Flexio-Ip-Transfer-S32k344-SPI-example-is-not-working/m-p/17...

0 Kudos
Reply
1,061 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

My colleague will communicate with you in your post. 

0 Kudos
Reply
1,126 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Which version of S32K3 RTD are you testing?

Since you are using S32K3X4EVB-Q257, do you use Pinmatrix to connect the SPI pins as mentioned in description.txt?

Lpspi_Flexio_Ip_Transfer_S32K344_RTD300P07 description.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,118 Views
lluo
Contributor III

Hi, Robin,

Thank you for your reply. We soldered extra wires on the board as shown in the circled area in the attached screenshot. And I am using s32 design studio 3.5. The S32K RTD  that I am using is RTD 4.0.0 D2311. Today I've tried to run the demo and it is working, though I still have no idea why the fault happened yesterday.  

0 Kudos
Reply
1,070 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

If you encounter the problem again, please tell me how to reproduce the problem so that I can test and check the cause.

0 Kudos
Reply
1,067 Views
lluo
Contributor III

noted. Thank you.

0 Kudos
Reply