Flash erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash erase

1,330 Views
wanghaitao
Contributor I
/* Specify the memory areas */
MEMORY
{
  /* APP从300KB开始,且总的APP区域 700KB */
  m_interrupts          (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00000400
  m_flash_config        (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000010
  m_text                (RX)  : ORIGIN = 0x00000410, LENGTH = 0x000AF000 - 0x00000410

  /* 标定参数区域从0x000AF000开始,且总的标定参数区域 64KB */
  m_calibration_rom     (RX)  : ORIGIN = 0x000AF000, LENGTH = 0x00010000

  /* SRAM_L */
  /* 从SRAM_L区域中划分标定参数区域 */
  m_data                (RW)  : ORIGIN = 0x1FFE0000, LENGTH = 0x00020000 - 0x00010000
  m_calibration_ram     (RW)  : ORIGIN = 0x1FFE0000 + 0x00020000 - 0x00010000, LENGTH = 0x00010000

  /* SRAM_U */
  m_data_2              (RW)  : ORIGIN = 0x20000000, LENGTH = 0x0001F000
}

 

/* 定义标定参数ROM区 */
  .calibration_rom :
  {
      . = ALIGN(4);
      calibration_data_rom_start = .;   /* ROM区域起始地址 */
      *(.calibration_rom)               
      calibration_data_rom_end = .;     /* ROM区域结束地址 */
      . = ALIGN(4);
  } > m_calibration_rom

  /* 定义标定参数RAM区 */
  .calibration :
  {
      . = ALIGN(4);
      calibration_data_ram_start = .;     /* RAM区域起始地址 */
      *(.calibration)
      calibration_data_ram_end = .;       /* RAM区域结束地址 */
      . = ALIGN(4);
  } > m_calibration_ram AT > m_calibration_rom

  calibration_data_rom_end = calibration_data_rom_start + (calibration_data_ram_end - calibration_data_ram_start);

测试代码

uint32_t test_addr = 0x000AF000;

    // S32K148的FLASH_DRV_EraseSector最小擦除扇区大小是 4KB
    status = FLASH_DRV_EraseSector(&g_flash_ssd_config, test_addr, 4096);

    // 验证擦除
    status = FLASH_DRV_VerifySection(&g_flash_ssd_config, test_addr, 4096 / 16, 1u);

    uint8_t data[8] = {0x07,0x77,0,0,0,0,0,0};
    // S32K148的FLASH_DRV_Program最小可写大小是8B
	status = FLASH_DRV_Program(&g_flash_ssd_config, test_addr, 8, data);
    // S32K148的FLASH_DRV_ProgramSection最小可写大小是1KB
    //flashResult = FLASH_DRV_ProgramSection(&g_flash_ssd_config, CANID_private_addr, 4096 / 16);

	uint32_t failAddr = 0;
    // 验证写数据
	status = FLASH_DRV_ProgramCheck(&g_flash_ssd_config, test_addr, 8, data, &failAddr, 1u);

如上,我想通过flash驱动擦除m_calibration_rom(0xAF000)区域,但是无法擦除。同样的擦除函数我可以擦除0xBF000区域(0xAF000 + 0x10000后的地址),请问各位大佬有何解决想法。我使用的MCU是S32K148。

0 Kudos
Reply
1 Reply

1,303 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @wanghaitao,

Can you read the error flags right after the FTFC command is finished (CCIF = 1)?

danielmartynek_0-1733916886360.png

 

Regards,

Daniel

 

0 Kudos
Reply