Flash Partitioning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Partitioning

1,053件の閲覧回数
sungjun
Contributor II

hello. NXP team.
I'm using S32k146.
A core secure operation occurred during flash partitioning.

Afterwards, I cannot download my sw via trace32.

The function performed before core secure operation is FLASH_DRV_EraseAllBlock.

What should I do?


sungjun_0-1718623450628.png

 

タグ(1)
0 件の賞賛
返信
1 返信

1,032件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @sungjun,

If Trace32 cannot mass erase the MCU, and it reports that the MCU is locked, it probably cannot be recovered.

Refer to AN12130 Production Flash Programming Best Practices for S32K1xx MCUs

https://www.nxp.com/docs/en/application-note/AN12130.pdf

Chapter 5 Common problems

 

It is also recommended to use the Erase All Blocks Unsecure FTFC command instead as it programs the FSEC byte to Unsecure.

danielmartynek_0-1718698874040.png

 

Regards,

Daniel

 

0 件の賞賛
返信