Fault Injection to cache locations using an interface provide in emcem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fault Injection to cache locations using an interface provide in emcem

78 Views
Rudved_3366
Contributor I

Hello @danielmartynek 

Good morning:-)

I have question regarding the fault injection to cache location:

I need to inject a 2-bit fault in Cache location but I'm not sure what it means as mentioned in the reference manual and we use NXP s32K394 microcontroller:

Rudved_3366_0-1791432690162.png

 

 

I need to call below function 2 times to inject the faults in cache and get the 2-bit error in cache like below: 

Rudved_3366_1-1791432699706.png

 

If I'm doing wrongly, could you please share the example code how to do this injection, and currently we are using SAF package in our project, so if there are already fault injection code exists for these, please share which file I need to refer to inject all kind of faults using (EIM) for memory test interface which is provided in SAF module.

0 Kudos
Reply
1 Reply

45 Views
danielmartynek
NXP TechSupport
NXP TechSupport
0 Kudos
Reply