FS85 INTB pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS85 INTB pin configuration

945 Views
sakshimashalkar
Contributor I

Hello Team, 

I am trying to configure with Infineon TC399 . I  am facing issue in configuring INTB pin . 

Can someone suggest how do we have to configure INTB pin or it will be handled by the device.

0 Kudos
Reply
1 Reply

917 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sakshi,

INTB is an open-drain active-low output with internal pull up (10kΩ) to VDDIO. When there is no fault or event, INTB is high (via this internal pull-up). When FS85 asserts an interrupt, INTB is pulled low. Each interrupt can be masked by setting the corresponding inhibit interrupt bit in M_INT_MASK registers.

On the MCU side, you should configure the GPIO connected to INTB as an input with interrupt capability on falling edge. In an interrupt handler, you should read M_FLAG registers over SPI to determine the cause and de-assert the interrupt pin.

BRs, Tomas

0 Kudos
Reply