FS32K116 Programming Problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS32K116 Programming Problems

1,394 Views
gary_yang
Contributor II

Dear Sir:

I am a third-party programmer manufacturer.

We have customers who successfully erase chip and program online using the J-Link user interface, but fail the FCT test.

未命名.jpg

However, they successfully mass erase and program online using the command line method, and both the programming and FCT tests succeed.

What are the differences between the user interface and command line methods for online programming? Or what could be the reason?

Attached is the command line log file.

 

Thanks

0 Kudos
Reply
3 Replies

1,081 Views
gary_yang
Contributor II

Dear Sir:

Our customer explained that after programming with J-Link, it's necessary to execute "Start Application." If it's not executed, onboard testing will fail.

螢幕擷取畫面 2026-03-10 163728.jpg

 What is the process involved in J-Link's "Start Application"? Or do you have any suggestions?

0 Kudos
Reply

1,074 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @gary_yang,

This is not an NXP tool, please contact SEGGER.

 

Thank you

0 Kudos
Reply

1,375 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @gary_yang,

This question is better directed to SEGGER technical support, as it involves their proprietary programming algorithm.
You can reach them here:

https://www.segger.com/support/technical-support/

 

BR, Daniel

 

0 Kudos
Reply