Example flexcan_encrypted_s32k144 does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example flexcan_encrypted_s32k144 does not work

Jump to solution
695 Views
David_Estevez
Contributor I

When sending data via CAN, the sending function is executed correctly and the CAN drivers return the value of "status success", however with the help of the oscilloscope you can see how the voltages of both Can_low and Can_high do not vary from 2, 5V in no time.

David_Estevez_0-1678362311249.jpeg

The board is connected to a peak Can as follows:

David_Estevez_1-1678362368024.jpeg

 

0 Kudos
Reply
1 Solution
675 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please follow the guide of example file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.3/doc/html_S32K144/flexcan_encrypted_...

How did you power the S32K144EVB?  Note: Power on the board with external supply 12V (J16)

FlexCAN Encrypted S32SDK_S32K1XX_RTM_4.0.3 S32K144.png

J107 should connect 1-2, otherwise how did you power S32K144.

J107 S32K144EVB.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
676 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please follow the guide of example file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.3/doc/html_S32K144/flexcan_encrypted_...

How did you power the S32K144EVB?  Note: Power on the board with external supply 12V (J16)

FlexCAN Encrypted S32SDK_S32K1XX_RTM_4.0.3 S32K144.png

J107 should connect 1-2, otherwise how did you power S32K144.

J107 S32K144EVB.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply