Ethernet PHY Over SPI Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet PHY Over SPI Example

3,219件の閲覧回数
Engietoday
Contributor I

Hello

 

I'm working on integrating an Ethernet PHY that uses SPI as its interface with the MCU. I see the example projects that utilize Eth module in Tresos are using MII interfaces instead. Are there any support material that might help shed some light on using SPI as its interface?

 

Thanks

0 件の賞賛
返信
1 返信

3,204件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as we do not offer Ethernet PHY with SPI interface then we will have no example for that. Moreover I do not know such devices, maybe Ethernet controller (MAC+PHY) with SPI. Anyway for SPI examples refer to SPI demos in Tresos or S32DS.

BR, Petr

0 件の賞賛
返信