Ethernet PHY Over SPI Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet PHY Over SPI Example

3,205 Views
Engietoday
Contributor I

Hello

 

I'm working on integrating an Ethernet PHY that uses SPI as its interface with the MCU. I see the example projects that utilize Eth module in Tresos are using MII interfaces instead. Are there any support material that might help shed some light on using SPI as its interface?

 

Thanks

0 Kudos
Reply
1 Reply

3,190 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as we do not offer Ethernet PHY with SPI interface then we will have no example for that. Moreover I do not know such devices, maybe Ethernet controller (MAC+PHY) with SPI. Anyway for SPI examples refer to SPI demos in Tresos or S32DS.

BR, Petr

0 Kudos
Reply