Error reporting module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error reporting module

12 Views
durga_choudhury
Contributor V

MCU: S32K148 in 144 pin package

RTD version: SW32K1_S32M24x_RTD_4.4_3.0.0_QLP03_D2507

S32 DS Version: 3.6.6

Target OS: Bare Metal

Host OS: Windows

 

With the above, I cannot find a module called "ERM" (or anything similar) in the driver module. I have looked in both both MCAL and Non-MCAL modules.

 

Is the ERM supported as a driver module or should the user manipulate raw pointers, as it used to be with the older 'Processor Expert' based framework?

0 Kudos
Reply
0 Replies